What is the Power Zone 200 Controller for Generac home standby generators?
This article provides an overview of the PowerZone 200 control panel, including its release, features, compatible models, operating modes, and connectivity options.
Need help with Mobile Link? Visit the Mobile Link support site.
This article provides an overview of the PowerZone 200 control panel, including its release, features, compatible models, operating modes, and connectivity options.
Provides troubleshooting instructions for the "Access Denied - You do not have a valid security token" error when connecting to a home standby generator through Field Pro. Covers internet connectivity, app version 1.14.2 or later, generator serial number verification, signing out and back in, reinstalling the app, and preparing for...
This article explains what to do when the Field Pro app displays FFFFFFFFFF instead of a generator's serial number. It provides separate support guidance for Independent Authorized Service Dealers and non-authorized installers or other users so they can contact the appropriate resource for assistance.
Explains how installers commission generators with a Power Zone 200 controller using the Field Pro mobile app, including the required on-site Bluetooth connection, registration, configuration, system testing, and activation. It also explains Mobile Link date and time behavior and optional ATS registration to help ensure the generator is...
This article explains how to configure or remove Wi-Fi backup for the Connectivity Cellular Accessory device using the Mobile Link or Field Pro app. It covers Bluetooth requirements, staying near the generator, troubleshooting connection problems, and removing Wi-Fi backup when needed to help reduce the risk of missed Mobile Link...
Fix the Field Pro message “Connected to another mobile device” when connecting to a Next Generation air-cooled standby generator with a PowerZone 200 control panel. This article explains why it happens and how to resolve it by ensuring only one device is connected, power-cycling the connectivity module, and reinstalling Field Pro, so you...
Learn how to view your generator firmware versions in the Field Pro app for Next Generation generators with the PowerZone 200 controller. This article explains how firmware updates happen through over-the-air FOTA when Wi-Fi or cellular is available, what to do if a firmware update is in progress too long, and what can block updates such...
This article explains how to prepare a Next Generation Series home standby generator for offline access using the Generac Field Pro app before a site visit with no Wi-Fi or cellular service. It walks through selecting “Prepare for a Future Visit,” finding and registering the generator if needed, and confirming the offline access window,...
If Product Registration shows “We couldn’t verify this address,” the address validation service may not recognize the address yet, such as in new development areas. Contact Generac Customer Support at 1-888-922-8482 to complete registration, then use Recheck registration status to confirm, for reliable registration status in the app.
This article provides troubleshooting steps for resolving Bluetooth connectivity issues between the FieldPro app and generators equipped with a PowerZone 200 controller. It includes checks for battery connection, proximity to the generator, LED status indicators, and proper cable connections.