Salesforce

Do I Have to Shut the Generator Down During Continuous Operation?

« Go Back
Fields
Do I Have to Shut the Generator Down During Continuous Operation?
Do-I-Have-to-Shut-the-Generator-Down-During-Continuous-Operation
Content
Yes, during extended outages, it is important to shut the generator down every 24 hours of operation to inspect the oil level and other maintenance items. See: Continuous use maintenance for home standby generators

Also see instructions for How to Shut Down the Generator When It’s Powering The House

Powered by