How long can I operate a portable generator? Does It Need a “Break”?
Our generators (including portables) are designed to run continuously, if needed, during extended outage scenarios. However, heavy use and long run times do require regular maintenance and operation checks, as well as following safe procedures when powering down your generator and disconnecting it from electrical loads.
Environment
This article applies to most Generac portable generators.
Continuous operation and Maintenance
-
Portable generators require an oil change after the initial break-in period, which varies depending on the engine. See your owner's manual for your generator's specific requirements.
-
After that, assuming you are running it continuously, we recommend checking the oil level and refilling it if necessary every time the unit runs out of fuel or every 8 hours, whichever comes first.
-
Additional maintenance intervals are outlined in your owner's manual.
How long can the generator run continuously?
When does the generator need maintenance?
Note: The maintenance schedule can be found in your owner's manual. Owner's manuals can be downloaded in PDF here.
-
Additionally, if you notice any signs of the unit running rough, stumbling, or making unusual noises, its important to shut it down immediately following the proper procedure before continuing operation. Addressing these issues promptly can prevent more serious problems.
Is there a proper way to shut down the generator during continuous operation?
-
When the unit is close to empty after a long run, you need to power down and disconnect all electrical equipment connected to it, then turn the generator off. This would be an ideal time to check oil levels as well, and then refill with fuel if necessary.
-
It is crucial to follow the proper procedure when shutting down a portable generator that is running under load. See the following article for more information on shutting down under load: Do I need to remove loads before shutting down my portable generator?
For information on continuous operation, running during an outage, and shutdown procedures for a stationary home standby generator see the following articles: