Adjusting generator exercise run time for standby generators
- For Next Generation air-cooled standby generators with a Power Zone 200 controller, the exercise period can be modified between 5 and 20 minutes. Note that this a Premium Mobile Link feature. The default exercise time is 5 minutes.
- Guardian-series air-cooled home standby generators have a non-adjustable 5-minute exercise period. While the exercise duration cannot be adjusted, the exercise schedule can be adjusted to run weekly, biweekly, or monthly. See What Is a Generator Exercise? article for more information.
Note: Some older models had a 12-minute exercise time. To confirm the exercise time for a specific generator model, reference the generator's user manual. See the Where can I download a user manual for my Generac portable generator? article for more information.