Calculating Fuel Costs
Several factors contribute to calculating the fuel expenses associated with operating a home standby generator, including:
- Load size and duration
- Size of the generator
- Ambient temperature
- Elevation at the geographical location of the generator
- Fuel type & price
- Pipe size
- BTUs required by the generator
Because of these varying factors it is recommended that prospective home standby generator owners reach out to an Independent Authorized Service Dealer or utility company to help determine the fuel cost.
BTUs
The generator's specification sheet or installation manual contains information regarding the fuel consumption rating for each fuel type in BTUs. These figures serve as a reference to estimate fuel costs. The specification sheets for a specific generator can be found on the product lookup page on Generac.com.