Salesforce

The Nexus and Pre-Nexus Control Panels

« Go Back
Fields
The Nexus and Pre-Nexus Control Panels
The-Nexus-and-Pre-Nexus-Control-Panels
Content

Nexus and Pre-Nexus Control Panels

Overview

The Nexus control panel was introduced on air-cooled home standby generators manufactured in 2010–2013. Generator controllers used on home standby systems manufactured before 2010 are referred to as “pre-Nexus” controllers.

Nexus Control Panel

Nexus control panel

  • Compatible with all connectivity device options
  • Functional in all Mobile Link applications
  • Limited command options
  • Sends status only
  • Exercise schedule setting available on most models
  • Accessories require a battery harness

Auto, Manual, and Off Modes

  • Auto – Automatically starts and provides power to the home with a loss of utility. See How Do I Put My Home Standby Generator Into Auto Mode? for more information.
  • Manual – Forces the engine to start, but will not provide electricity to the home unless the power fails.
  • Off – The unit is off and will not start with loss of utility.

LCD Screen

The LCD provides information about the generator’s status and condition.

  • Alarms – Stop the engine and prevent it from starting unless cleared by the user.
  • Error codes – Numerical value identifying the alarm/warning.
  • Warnings – Identify maintenance requirements or potential problems. Warnings will not prevent the unit from running.

Other Features

Pre-Nexus Control Panel

Pre-Nexus control panel

The pre-Nexus control panel was used on air-cooled home standby generators manufactured before 2010.

  • Compatible only with the Mobile Link 4G LTE cellular accessory
  • Functional only in the Mobile Link Consumer App
  • No command options
  • Exercise schedule setting available on limited models

Auto, Manual, and Off Modes

  • Auto – Automatically starts and provides power to the home with a loss of utility. See How Do I Put My Home Standby Generator Into Auto Mode? for more information.
  • Manual – Forces the engine to start, but will not provide electricity to the home unless the power fails.
  • Off – The unit is off and will not start with loss of utility.

LCD Screen

The LCD provides information about the generator’s status and condition.

  • Alarms – Stop the engine and prevent it from starting unless cleared by the user.
  • Error codes – Numerical value identifying the alarm/warning.
  • Warnings – Identify maintenance requirements or potential problems. Warnings will not prevent the unit from running.

Other Features

  • 7.5A automotive-style fuse – Protects cranking and running circuits. The engine will not start if this fuse is blown or missing.

See also


Powered by