Salesforce

What Do the Different Colors of LED Lights On My PWRcell Battery Mean?

« Go Back
Fields
What Do the Different Colors of LED Lights On My PWRcell Battery Mean?
What-Does-the-Different-LED-Color-Lights-On-My-PWRcell-battery-mean
Content

Environment

This article applies to PWRcell products. For LED status indicators on home standby generators, see the What Do the Green, Yellow, and Red Status Indicator Lights Mean on Home Standby Generators? article.
 

PWRcell Battery LED Indicator Lights

Note: LED indicator patterns will vary depending on firmware type. Systems that are connected will have the latest firmware. Reference your user manual for patterns and troubleshooting steps specific to your model.

Every LED color and sequence on your battery cabinet has its own specific meaning. The different colors are as follows: 
 
  • Orange, Solid - Disabled. The battery cannot be in use until it is enabled.
  • Orange, strobe (2s) - Waiting. Check the battery disconnect switch. Try disabling and enabling the battery using the inverter screen. Please consult your PWRcell battery owner's manual for further troubleshooting: 
  • Green/ Orange, alternating - Initializing. The battery is trying to connect. This light is often seen if you are performing a black start on your battery. 
  • Green, Solid - Charging-The battery is currently charging from solar power or the grid. 
  • Green, Rapid Blinking (0.5s) - Discharging. The battery is currently providing power to your home or back to the grid. 
  • Green, Strobe (2s) - Standby - The battery is currently waiting for an outage to occur. 
  • Red, Rapid Blinking - Error - This could be multiple different errors depending on the situation. Please contact Customer Support
  • Red, Strobe - Sleeping - The battery has reached the absolute minimum state of charge that is set on your system. It will sleep for one hour, then turn on for another four minutes to perform a powerful search. This will occur until the battery senses a source of power from the PV links or another source of energy. Once established, it will start charging/ discharging again. During this time the inverter will be turned off and the protected loads will no longer receive power. 

image.png

image.png

Powered by