Integrated sediment trap
Beginning with the 2016 model year, Guardian series generators include a factory-integrated sediment trap. This feature is also standard on Next Generation series generators.
Environment
This article applies to:
- Guardian series generators manufactured in 2016 and later
- Next Generation series generators
Sediment trap details
- Designed to prevent unwanted particles or debris from entering the fuel regulator and engine.
- Factory-integrated on each unit, eliminating the need for installers to build one in the field.
- Ensures all units have a properly built sediment trap.
- Saves installation time and materials.
- The sediment trap should be cleaned as part of regular maintenance. For steps, see: How Do I Clean the Sediment Trap in a Generac Air-Cooled Home Standby Generator?
Sediment trap locations
Image of sediment trap on a Guardian series generator:

Sediment trap location on Guardian series generators (from owner’s manual):

Sediment trap location on Next Generation series generators (from owner’s manual)