What Type of Fuel Should I Use in My Portable Generator?

Generac portable generators are equipped with 4-stroke engines that require clean, fresh, unleaded gasoline. It's important to use fuel with a minimum rating of 87 octane and no more than 10% ethanol.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support