Why Didn't Power Switch Over to the Generator After Losing Utility Power?

The transfer of power relies on the 194/23 wires that form the power transfer circuit. If these wires are not connected, or the generator cannot supply the 12v 194 wire with power, then the transfer will not occur.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support