Can I Use E85 Fuel in My Portable Generator?

E85 fuel should never be used. Generac portable generators are equipped with 4-stroke engines that require clean, fresh, unleaded gasoline. It's important to use fuel with a minimum rating of 87 octane and no more than 10% ethanol. Any modification to an engine's fuel system will put the unit's warranty at risk.

Title
Can I Use E85 Fuel in My Portable Generator?
URL Name
Can-I-Use-E85-Fuel-in-My-Portable-Generator

Public Answer
Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support