Can I take out the generator's main breaker and replace it with a larger breaker?

The breaker that is pre-installed on a generator is sized for the unit's output capabilities. Replacing a breaker with a larger breaker will not yield any more output of the unit, and would allow the unit to be easily overloaded. This modification would also void the unit's warranty.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support