Can I use a portable or home standby generator to charge my electric vehicle (EV)?

The article discusses the use of portable generators to charge electric vehicles. Level 1 chargers, which require between 1000-2000 watts of power, can be powered by most portable generators. However, for Level 2 charging, which requires a 120/240-volt 50-amp receptacle and can require up to 9600 watts of power, users will need to carefully consider the compatibility between their intended EV charging system and the portable generator being used.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support