Can the supported voltage of an automatic transfer switch be adjusted?

This article explains that an automatic transfer switch’s supported voltage and phase are fixed ratings and cannot be changed to match a different site service, such as 120/240 single-phase versus 120/208 three-phase. It helps clarify what customers mean by “changing voltage,” including when they are actually asking about pickup and dropout voltage thresholds. Use an Independent Authorized Service Dealer to scope the site requirements and select the correct ATS from the start for safe, reliable transfers.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support