High elevation home standby generator installation FAQ
This article provides information on considerations and FAQs related to installing Generac home standby generators at high elevations above 2,000 ft. Some of the concerns mentioned include the need to adjust the engine configuration, potential reduction in power output, and the availability of high altitude kits.