How Long Does It Take To Recharge the GB Series Portable Power Stations?

Using the built-in AC charging adapter that is included with the unit, the GB1000 - 0-80% recharge time is about 2.1 hours. The GB2000 - 0-80% recharge time is about 4 hours. Fast-charging accessories are available (Model Numbers: 8031 and 8030) which can improve charge speeds. 

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support