How do I add a power station to the Generac Go app?
Learn how to add and pair a compatible Generac GB power station with the Generac Go app using Bluetooth or 2.4 GHz Wi-Fi. Bluetooth allows local control without an account, while Wi-Fi requires an account for remote monitoring, push notifications, and firmware updates. Includes troubleshooting steps when a power station won't appear, pair, or connect to the app. Legacy GB1000 and GB2000 models are not compatible. Follow these instructions to establish reliable connectivity and manage your power station.