How do I connect or reconnect my power station to Wi-Fi in the Generac Go app?
Learn how to connect or reconnect a compatible Generac GB power station to a 2.4 GHz Wi-Fi network using the Generac Go app, including after changing Wi-Fi networks or passwords. Find troubleshooting steps when Wi-Fi networks do not appear, and understand how Wi-Fi enables remote monitoring, notifications, and firmware updates while Bluetooth provides local control. The GB1000 and GB2000 are not compatible with the Generac Go app. Follow these steps to maintain reliable connectivity.