How do I toggle my charger’s LEDs on and off?This article guides users on how to toggle their charger's LEDs on and off.Nov 18, 2025Knowledge
FieldsTitleHow do I toggle my charger’s LEDs on and off?URL NameHow-do-I-toggle-my-charger-s-LEDs-on-and-offContentPublic ContentHow do I toggle my charger’s LEDs on and off? The Generac charger's LEDs are always on by default, but you may need to switch them off for various reasons.Level 2 Plus (running firmware version 5.11 or higher) LEDs can be switched off anytime with the Generac EV Charging app. 1. Log in to the Generac EV Charging app by filling in your credentials.2. Connect to your charger by Bluetooth and stay close to the charger during all the following steps. You can only turn the charger’s LED off or on by being connected to the charger via Bluetooth. A pop-up will ask you to switch to a Bluetooth connection if you are connected to your charger via Wi-Fi rather than Bluetooth. 1. Select your charger in the app.2. Tap the cogwheel icon in the top right corner to access the charger’s settings.3. Tap Advanced options.4. Set the “LED Always on” switch to the off position to turn off the LED. Follow the same step to switch it back on.5. Tap Save. Once you turn the “LED Always on” switch to the off position, the LED will still be lighting while the action is performed but will turn off after 8 seconds without interaction.
Was this article helpful?Choose a general reason-- Choose a general reason --FeedbackUpload FilesUpload FilesOr drop filesSubmit