How to adjust the Level 2 Plus charging current
To avoid circuit overloading, electric vehicle owners with a charger on a high voltage circuit should reduce the amperage when other appliances are also in use. There are two ways to manage the charger's current, either by setting the current selector switch during installation to ensure neither the charger nor the vehicle draws more than 80% of the circuit's maximum rating, or by using the Generac EV Charging app to adjust the current at which the car will charge. However, make sure you are not exceeding the maximum power capacity of your charger set by your installer.