If the Generator Is Being Used, How Do I Connect or Disconnect Electrical Devices?

NEVER start or stop the generator's engine with running electrical devices plugged into the generator. When the generator is turned off, you can only connect electrical devices that are turned off. When the generator is turned on, you may connect electrical devices that are turned on or off.

Title
If the Generator Is Being Used, How Do I Connect or Disconnect Electrical Devices?
URL Name
If-the-Generator-Is-Being-Used-How-Do-I-Connect-or-Disconnect-Electrical-Devices

Public Answer
Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support