What are the included features on the air-cooled home standby enclosures?

This article explains the key features of Generac air-cooled home standby generator enclosures, which protect the generator from weather, debris, and corrosion while reducing noise. It covers both the Next Generation (10–28 kW) and Guardian (10–26 kW) Series models, detailing their aluminum construction, sound-attenuated, weather-resistant design, and sloped-roof airflow system. Additional highlights include the composite mounting base, external emergency shutdown switch, LED status indicators, Wi-Fi and Mobile Link® connectivity, and simplified service access. Customers searching for “air-cooled generator enclosure features,” “home standby generator housing,” “generator aluminum enclosure,” or “Generac Guardian vs. Next Gen enclosure” will find a complete comparison and specifications here.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support