What Are the Main Differences between Clean Water, Semi-trash, Trash, and Chemical Pumps?

Clean water and chemical pumps typically have carbon ceramic mechanical seals, while semi-trash and trash pumps have silicon carbide mechanical seals. Trash pumps use a 2-vane impeller design, allowing larger particulates to pass through without damage, whereas clean water and chemical pumps use a 4-vane design. Internal components of chemical pumps feature fiberglass reinforced nylon to resist corrosion.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support