What Does It Mean When My Generator Displays an Error Code: Auxiliary Shutdown, Error Code 2800?

This error indicates that one or both of the auxiliary shutdown switches is in the OFF position. One switch is located on the back of the generator, and generators rated at 15kW and greater will have a second shutdown switch inside the generator housing on the firewall panel. Both of these switches must be on or else the generator will not run.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support