What Does It Mean When My Generator Displays an Error Code: Fuse Problem, Code 2400?

This error indicates that the 7.5A fuse is missing or blown. Check to confirm if the fuse is in place or has been blown. The fuse is located on the generator control panel, underneath a rubber flap.

Title
What Does It Mean When My Generator Displays an Error Code: Fuse Problem, Code 2400?
URL Name
What-Does-It-Mean-When-My-Generator-Displays-an-Error-Code-Fuse-Problem-Code-2400

Public Answer
Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support