What Does It Mean When a Transfer Switch Is NEMA 1 Rated?

When a transfer switch is NEMA 1 rated, it means that the switch is designed for indoor use and provides a degree of protection against accidental contact with live electrical parts. Specifically, a NEMA 1 rated transfer switch provides protection against incidental contact with the enclosed equipment and protects against the ingress of solid foreign objects, but does not provide protection against moisture or other environmental factors.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support