What Is an Automatic Transfer Switch (ATS)?

An Automatic Transfer Switch (ATS) is an electrical switch that automatically transfers power from the primary source (utility power) to a secondary source (backup generator) when it senses a power outage or interruption in the primary source. It is commonly used in home standby generator systems to ensure continuous power supply to critical loads in buildings, hospitals, data centers, and other facilities. The ATS monitors the power supply and automatically switches between the primary and secondary sources, allowing for uninterrupted power supply during power outages or other disruptions.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support