What Is the Difference between a NEMA 1 and NEMA 3R Rated Transfer Switch?

The main difference between a NEMA 1 and NEMA 3R rated transfer switch is the level of protection they provide against environmental conditions. A NEMA 1 rated transfer switch is intended for indoor use and offers basic protection against dust, falling dirt, and dripping water. In contrast, a NEMA 3R rated transfer switch is intended for outdoor use and offers protection against rain, sleet, snow, and ice formation. It also provides a degree of protection against windblown dust and the ingress of solid foreign objects. Therefore, if you plan to install a transfer switch outdoors, a NEMA 3R rated switch is recommended.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support