What is the layout of the control wires and what do they do?

In a Generac Home Standby Generator installation, control wires play an essential role in allowing proper communication between the generator, transfer switch, and utility power source. The N1/N2, T1, 23/194, and 0/DC Common wires are key control wires that must be properly connected for optimal performance, and regular maintenance checks are critical to ensure reliable generator operation.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support