Core Power VS PowerPact: control panel differences

This article explains the differences between Core Power 7 kW (2007–2013) and PowerPact 7.5 kW (2013–2024) home standby generators, focusing on operating modes and weekly exercise behavior. It clarifies how to select Auto, Manual, and Off using either a rocker switch or dedicated buttons, and how to set the 7-day, 12-minute exercise with the Set Exercise button. Use this guide to confirm controls, adjust exercise time, and understand the 7.5 A fuse function for reliable operation.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support