What is the maximum temperature of water that my pressure washer can handle?

100 degrees Fahrenheit is the max temperature for the water supply for all Generac pressure washers. They are equipped with a Thermal Relief Valve that will disperse the water at 125F to protect against the pump failing.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support