Why Did My Portable Generator Just Stop Working?
If the generator has been running effectively without any signs of trouble and stops all of a sudden, check to ensure there is sufficient levels gas and oil. If generator has appropriate fuel levels, check to see if a circuit breaker are tripped. The generator may have shut down because of overload, which can damage its internal components. In this situation, you need to reset the circuit breakers and power fewer appliances with it. If the problem is not resolved, then there may be something wrong with the generator itself. You should have a Generac Service Dealer inspect it and provide repair.