Why Does My Automatic Transfer Switch (ATS) Have a Larger Breaker Than My Generator Breaker?
A generator’s main breaker is sized to handle the rated amperage of the generator and is intended to protect the generator from being overloaded. When using a whole house transfer switch the transfer switch amperage should match the amperage rating of the panel that it is protecting.