Why would the N1/N2/T1 fuses blow during installation?
The fuses for N1/N2/T1 can blow during installation due to a surge of power from utility, or due to improper handling of the wires during installation. The fuses should be replaced if blown. Do NOT use a fuse with a higher amperage when replacing as this can lead to damage that is not warrantable.