Salesforce

How Do I Check the Signal My Mobile Link Device Is Seeing?

« Go Back
Fields
How Do I Check the Signal My Mobile Link Device Is Seeing?
How-Do-I-Check-the-Signal-My-Mobile-Link-Device-Is-Seeing
Content

In the Mobile Link app or website (whichever you prefer to use) this will be displayed on the generator card/box when you first login.
 

Checking signal strength in Mobile Link

Signal strength is displayed in the upper left of the generator tile in the Mobile Link web or mobile app.

image.png

In the mobile app, tap the generator card to view the generator details. 

image.png
 

Signal reference guides: 

Note: Keep in mind that the lower the signal the slower the updates will be. We recommend improving the signal as much as possible. This could entail removing any signal blockers that may be in the way or interfering.  

Note: Signal readings update every 24 hours in the app. If a changes in your signal you may see a change in the percentage displayed at the time of the signal reading update. 

 

Checking signal strength using the generator controller

1. Click the off button on the generators control panel.
2. Hit escape button.
3. Use the down arrow until you see Wi-Fi flashing and hit enter.
4. The first option should display signal.


Powered by