Understanding the home standby generator's battery charging system

This article explains how Generac home standby generators (10–28 kW air-cooled with Power Zone 200, Evolution/Evolution 2, or Nexus controls, plus some liquid-cooled models) keep the starting battery charged using the built-in charger and the 120 VAC T1 charging circuit. It covers normal, temperature-compensated charging voltage and the automatic 18-hour charge cycle, plus what “Inspect Battery” or “Charge Warning” may mean. You’ll also learn common causes of a no-charge condition, like loss of T1 power, a blown ATS fuse, or missing neutral, to help support reliable starting and operation.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support