What is the T1 fuse in my transfer switch?

The T1 circuit in Generac automatic transfer switches provides 120VAC power to keep the generator’s battery charged. In single-phase models, this circuit includes a fused T1 connection located inside the ATS and should only be serviced by trained personnel. Three-phase transfer switches do not have a T1 fuse and instead require a dedicated 120VAC protected circuit from the main panel.

Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support