Understanding the home standby generator's battery charging system

This article explains how Generac home standby generators (10–28 kW air-cooled with Power Zone 200, Evolution/Evolution 2, or Nexus controls, plus some liquid-cooled models) keep the starting battery charged using the built-in charger and the 120 VAC T1 charging circuit. It covers normal, temperature-compensated charging voltage and the automatic 18-hour charge cycle, plus what “Inspect Battery” or “Charge Warning” may mean. You’ll also learn common causes of a no-charge condition, like loss of T1 power, a blown ATS fuse, or missing neutral, to help support reliable starting and operation.

Title
Understanding the home standby generator's battery charging system
URL Name
How-Is-My-Home-Standby-Generator-Battery-Charged

Public Answer
Was this article helpful?
Upload Files


Need more help? Get in touch with our support team.


Contact Support