Connect a generator to your home Wi-Fi network with the Mobile Link app (Android)
Generator owners can connect their generators to their home Wi-Fi network using a setup wizard within the Mobile Link for Generators mobile app. Once connected, this app allows users to monitor their generator and change certain generator settings.
Experiencing frequent Wi-Fi disconnections? Upgrading to the Connectivity Cellular Accessory is recommended for users who wish to add connectivity to their generator or users experiencing ongoing connectivity issues. It is compatible with more generators and uses multiple carrier networks to offer greater coverage. Basic (free) and Premium cellular plans are available for users of this device. See here to upgrade: Connectivity Cellular Accessory
Do I need to create an account and sign up for a Mobile Link subscription?
Creating a Mobile Link account is not required to connect the generator through the app. The connection wizard is available without signing in. Generac support recommends attempting the connection process first to confirm reliable network connectivity before subscribing to a Premium Mobile Link plan.
Before purchasing a subscription, homeowners should ensure that their generator has a reliable cellular or Wi-Fi connection. Refunds are not available for issues caused by poor connectivity. A Mobile Link device is required. For details, see the Mobile Link Wi-Fi, Cellular, and LTE device compatibility guide.
Setting up a separate SSID for your 2.4 GHz network is strongly recommended to maintain a stable connection.
Struggling to connect or stay connected?
Check network settings: Verify that your network meets the requirements outlined in this article to resolve most connectivity issues
Consider upgrading to cellular: Upgrading to the Connectivity Cellular Accessory is recommended for users who wish to add connectivity to their generator OR for users experiencing ongoing connectivity issues. It is compatible with more generators, and uses multiple carrier networks to offer greater coverage. Basic (free) and Premium cellular plans are available for users of this device. See here to upgrade: Connectivity Cellular Accessory.
Video instructions
Prepare the generator control panel for connection to a Wi-Fi Network:
1. Go to the generator, unlock it, and raise the cover to the generator. 2. Locate the control panel on the right side of the open generator, then press the OFF button on the control panel.
Note: The control panel is the display screen and series of buttons pictured below.
Note: The generator needs to be in the off mode (SWITCHED TO OFF) to access the Wi-Fi pairing mode and to ensure that the generator does not attempt to start during this process. The Final Steps section of this article will ensure the generator is returned to a READY TO RUN state after connecting.
3. Press the ESCAPE button to access the control panel's main menu.
4. Using the up and down arrow keys above and below theENTER button, press the down arrow to select the WIFI or SET UP WIFI option, then press the ENTER button.
or
5. After pressing the ENTER button on WIFI or SETUP WIFI, the screen will display one of the following:
If SETUP WIFI? is displayed, use the arrow keys to select YES and then press the ENTER button.
If something other than SETUP WIFI? is displayed, use the arrow keys to scroll until REDO WIFI SETUP? NO is displayed, and press the ENTER button. Next, use the arrow keys to scroll until YES is displayed, and press the ENTER button again.
If SEARCHING is displayed on the control panel, follow the steps in the sentence above to scroll up and redo the Wi-Fi setup.
6. The generator's control panel should now display SET TO AP - Please Wait... After two to three minutes, the screen should change and display SETUP WIFI NOW!
7. Once the screen displays SETUP WIFI NOW! the generator is ready for connection. See below to continue the setup in the app.
Note: A timer and a number beginning with MLG will alternate on-screen. This is normal. The MLG number will be referenced later in this process, and it may be helpful to write it down. See How Do I Find the WI-FI SSID on My Generator's Control Panel? for more information.
Connect a generator to WiFi using an Android Device:
7. A What does the display on your generator say? screen will appear. Select the Setup WIFI Now! Timer counting down/SSID name shown option. If the generator control panel does not display "Setup WIFI Now!" option, select the matching option shown in the app.
8. A Wait until you see a timer... screen will appear. Verify that a timer and MLGXXXXX are rotating on the generator's control panel screen, then tap the Yes, connect now button.
Note: If the control panel fails to alternate between a countdown timer and MLGXXXXX it may need to be reset. Continue through the connection process first. If issues persist, see the How Do I Perform a Hard Reset on a Home Standby System? article for more information.
9. Mobile Link will begin searching for a nearby MLG network. This may take a few seconds. Please wait for up to thirty seconds for the app screen to advance.
10. A prompt will appear requesting permission to connect the phone to the generator's temporary network. Verify that the MLG number listed on the phone screen matches the MLG number shown on the control panel's display, then click Connect.
11. Within a few seconds, the app will indicate that the connection to the temporary MLG network is established.
12. The app will request confirmation of the MLG network name. Verify that the displayed MLG network name is correct, and tap the Continue button.
13. A list of available Wi-Fi networks should be displayed. Select the Wi-Fi network name to which the generator should be connected.
Note: If a list does not automatically appear, tap the Refresh list of available networks option, the app will rescan for available networks in the area. See Is My Wi-Fi Network Compatible With Mobile Link? for more information.
14. Enter the password for the Wi-Fi network that was selected in the previous step, then press the Submit button.
15. Within a few moments, the Configuration sent screen will appear. The generator has now been successfully connected to the selected Wi-Fi Network, however, it may take up to 15 minutes for information to update in the Mobile Link app. Next steps are provided within the phone app. These next steps are also described in greater detail in the Final Steps section provided below.
Final Steps
1. Wait for the generator screen to say NOW CONNECTED, then press the ENTER button to continue. This typically happens within three to four minutes or less, but can sometimes take up to fifteen minutes.
2. The generator screen will display the signal strength. Verify that the signal strength is acceptable, then press the ENTER button.
Note: Signal strength of 30% or greater is recommended. If lower than 30% signal strength is observed, consider adding a Wi-Fi booster or Extender to your network to improve connection reliability. See the What should I do if I have a weak Wi-Fi signal strength? article for more information.
3. The generator control panel will display the Timezone.Select the correct timezone, then press the ENTER button to continue.
Note: If PLEASE SELECT HOUR is displayed, wait a few moments for the timezone information to be displayed. Alternatively, the current date and military time can be entered manually using the arrow keys.
4. After confirming the time or time zone, the display should return to the Main Menu. Using the arrow keys, select the SYSTEM option, then press the ENTER button.
Note: After selecting the time or timezone, if the screen displays something other than SYSTEM and the main menu, press ENTER or ESCAPE to return to the main menu. Then, select the SYSTEM option, and press the ENTER button.
5. The screen will display SWITCHED TO OFF. Press the AUTO button.
6. The generator should return to the READY TO RUN HOURS OF PROTECTION. The generator is prepared for the next outage.
7. Press the EXIT SETUP button in the app. The generator is connected to Wi-Fi and ready for remote monitoring.
If your generator will not connect to Wi-Fi, follow the steps below. Many issues are resolved by verifying the network type, improving signal strength, or re-running the connection in the Mobile Link app.
Note: Mobile Link Wi-Fi devices operate on 2.4 GHz only (802.11 b/g/n). Dual-band and mesh systems may require a dedicated 2.4 GHz SSID during setup.
Can’t see your home network (hidden SSID)? Use the Mobile Link option to enter the SSID manually. See Connect when SSID is hidden.
App or controller stuck during setup? If the Mobile Link app won’t load, try the steps in Mobile Link app won’t load. If the controller shows “Set to AP, please wait…”, see “Set to AP” is stuck.