Quiet Test Mode
Quiet Test Mode (also referred to as Low Speed Exercise Mode) runs the generator at a lower RPM during the scheduled exercise cycle, which results in a quieter run. Quiet Test Mode is recommended to generator owners who prioritize quiet generator operation. Quiet Test Mode is not available on all generator models.
Environment
This article applies to Generac air-cooled home standby generators.
For Next Generation Series generators, see here.
For Guardian Series generators (2017-present), see here.
- Launch the Mobile Link app on your phone or in the web browser. Click or tap the generator tile.
- Click or tap Exercise Settings, select Exercise Schedule.
- In the Exercise Schedule screen, you will find a toggle switch for Quiet Test Mode underneath the Exercise Duration slider. Toggling this switch to the right will enable Quiet Test Mode. Clicking on the question mark icon will explain Quiet Test Mode. You can also find this information in the Exercise FAQ's section.
- Make sure to SAVE your settings when you are finished.
Note: Enabling Quiet Test Mode through the Mobile Link App is only available for generators with the PZ200 controller at this time.
At the generator lift the lid to access the control panel. Quiet Test Mode is enabled within the EXERCISE TIME menu.
- Press OFF.
- Press ESC.
- Arrow down to the Sub Menus and hit ENTER.
- Arrow to the Edit menu and hit ENTER.
- Arrow to the Exercise Time menu and hit ENTER.
- Choose the exercise frequency and hit ENTER.
- Toggle YES to enable QUIET TEST MODE? and hit ENTER.
Note: If the Quiet Test Mode option is not available, then the generator does not support this feature.