Read the manual thoroughly and understand all of the instructions, cautions, and warnings before using this equipment. If any section of the manual is not understood, contact your nearest authorized dealer, or contact Generac Customer Service at 1-888-436-3722 (1-888-GENERAC), or www.generac.com with any questions or concerns.
Installing the Generac Connectivity Cellular Accessory
This article provides complete instructions on how to install the Generac Connectivity Cellular Accessory on air-cooled and liquid cooled home standby generators with a compatible controller. To determine if your generator's controller will work with the Generac Connectivity Cellular Accessory, see here: Which generator controllers are compatible with Wi-Fi or LTE cellular Mobile Link connectivity devices?
Environment
This article provides instructions on how to install the Generac Connectivity Cellular Accessory. For instructions on how to install the 4G LTE device, see here: How Do I Install the Mobile Link 4G LTE Device on My Home Standby Generator?
Installation instructions
- Download this file for installation instructions.
- The installation process will vary depending on whether you have an air-cooled or liquid-cooled generator, and whether this is a Mobile Link device replacement or a new accessory installation.
When ordering a Connectivity Cellular Accessory kit (G0072150) for a Liquid-Cooled (LC) generator built before November 2024, you will need to order an additional harness (part number A0005166075). This applies to these generators:
- RG02515
- RG03015
- RG04845
- RG06045
- RG08045
- RG10090
- RD03022 (will also need G0064780/0K2231)
- QT series (can also use G0064780/0K2231)
For the RG130 and RG150, you will need a different harness A0005792571 due to the size of the generator. This applies to these generators:
The harness included with the Connectivity Cellular Accessory kit is A0005914366. This is not needed for these generators. This can be saved and used on LC gens.
If you have any questions about the installation, we recommend you contact a Generac authorized service dealer.
Configure Wi-Fi backup for your device
How do I set up Wi-Fi for my Connectivity Cellular Accessory?
How do I change the Mobile Link device in my Mobile Link account?
If you recently installed a replacement Mobile Link device on your generator and need to add it to your Mobile Link account, contact your preferred Generac dealer or Mobile Link Support (855-436-8439) with the device serial number and generator serial number.
Your dealer or Mobile Link Support will then update the device in your Mobile Link account.