Mobile Link Wi-Fi Kit
This Wi-Fi kit is a self-installation kit for compatible home standby generators that did not come with a factory-installed Wi-Fi module due to a supply shortage. If your unit is one of the affected units, you will have paperwork with the generator. If you are not sure, please feel free to contact customer service at 855-436-8439. Note that this Wi-Fi Kit is not the same as the Wi-Fi/Ethernet or 4G/LTE aftermarket accessories, which are now discontinued. For more information about Mobile Link devices, see: Mobile Link Wi-Fi, Cellular, and LTE device compatibility guide
Note: Upgrading to the Connectivity Cellular Accessory is recommended for users who wish to add connectivity to their generator or users experiencing ongoing connectivity issues. It is compatible with more generators and uses multiple carrier networks to offer greater coverage. Basic (free) and Premium cellular plans are available for users of this device. See here to upgrade: Connectivity Cellular Accessory.
Compatible generators
All of the following must be true:
- Manufacture date is approximately after May 2021
- Air-cooled generators only with an Evolution 2.0 controller
- Air-cooled generators 10Kw- 24Kw
Request form
If your generator is eligible for the Wi-Fi kit, complete this form: https://www.generac.com/wifikit