Salesforce

Mobile Link Wi-Fi keeps disconnecting

« Go Back
Fields
Mobile Link Wi-Fi keeps disconnecting
Mobile-Link-Wi-Fi-keeps-disconnecting
Content

Discontinued Notice: The Wi-Fi/Ethernet accessory has been discontinued. Upgrading to the Connectivity Cellular Accessory is recommended for users who wish to add connectivity to their generator or users experiencing ongoing connectivity issues. It is compatible with more generators and uses multiple carrier networks to offer greater coverage. Basic (free) and Premium cellular plans are available for users of this device. See here to upgrade: Connectivity Cellular Accessory.

Wi-Fi keeps disconnecting

Wi-Fi networks can suffer from many failure points, and you may not notice this until you are proactively monitoring something that is connected to it (the generator is a great example). In some scenarios, you may notice that your generator is not able to maintain a stable Wi-Fi connection with your home's Wi-Fi network.

Environment

Mobile Link Wi-Fi devices: This article applies to the onboard Wi-Fi device and the Mobile Link Wi-Fi/Ethernet aftermarket accessory. For more information, see: Mobile Link Wi-Fi, Cellular, and LTE device compatibility guide

When should I contact my ISP?

There can be a variety of reasons this may occur, including but not limited to the items below. If you have concerns about your generator (or other devices) not maintaining a connection, we urge you to work with your internet service provider (ISP). Some causes are outside of the ISP’s control; however, they can identify certain issues (like line problems or router/modem malfunctions) that could be contributing factors.

Mobile Link connection details

  • Mobile Link checks in with your internet service and router every 15 minutes.
  • If the router and internet service fail to respond, Mobile Link will continue trying every 15 minutes.
  • If no response is received within 3 hours, Mobile Link will switch from online to offline status.
  • If enabled, the no signal notification is sent after 48 hours of no response from the router.

Common causes of disconnection

  • Important: Mobile Link Wi-Fi devices require a dedicated 2.4 Ghz network. For more information, see: Is My Wi-Fi Network Compatible With Mobile Link?
  • Internet outage
  • Mesh networks 
  • Router has reached the maximum number of connected devices
  • Heavy bandwidth usage from other devices
    • Security systems (e.g., Ring, Blink)
    • Streaming video or audio
  • Signal changes or fluctuations
    • Run regular speed tests and share data with your internet provider
  • Changes in physical signal blockers, including:
    • Metal (including metal blinds)
    • Doors and furniture
    • Walls or buildings (especially concrete, steel, and brick)
    • Water (e.g., fish tanks)
    • Nearby routers or modems
  • Wi-Fi extenders may power down due to inactivity (power-saving settings)
  • Location on the internet line (beginning, middle, or end)
    • If you are in the middle or end of the line, devices ahead of you may impact your connection

Still experiencing unreliable Wi-Fi connection?

The Cellular Connectivity Accessory provides more reliable network through the use of multiple cellular carriers. A free plan is also available for this cellular device.


Powered by