Generator controller functionality and commands
Mobile Link product compatibility and feature support are heavily dependent on the control panel type that the generator uses. Below is a current breakdown of compatible devices and which commands can be sent for each control panel.
Sections
Power Zone 200 controller
See: What is the PowerZone 200 Controller for Generac home standby generators?
Power Zone 410 controller
See: What is the Power Zone 410 controller?
Evolution 2.0 / Sync 3.0 controller

Note: The Evolution 2.0 and Sync 3.0 controllers are similar in operation and functionality. The Evolution 2.0 controller is used on Generac generators, while the Sync 3.0 controller is used on Honeywell generators.
- Compatible with all connectivity device options
- Functional in all Mobile Link Applications
- Full Command Options
- Fault
- Maintenance
- Exercise
- Send Status
- Exercise Schedule Setting
- Accessories DO NOT require a battery harness
Note: For additional information on the Evolution controller, and key differences between Evolution 1.0 and Evolution 2.0, see What is the Evolution controller for Generac home standby generators?
Evolution 1.0 controller
Note: The Evolution 1.0 and Sync 2.0 controllers are similar in operation and functionality. The Evolution 1.0 controller is used on Generac generators, while the Sync 2.0 controller is used on Honeywell generators.
- Compatible with all connectivity device options
- Functional in all Mobile Link Applications
- Limited Command Options
- Exercise Schedule Setting
- Accessories REQUIRE a battery harness
Note: For additional information on the Evolution controller, and key differences between Evolution 1.0 and Evolution 2.0, see What is the Evolution controller for Generac home standby generators?
Nexus controller

- Compatible with all connectivity device options
- Functional in all Mobile Link Applications
- LIMITED Command Options
- Exercise Schedule Setting available on MOST models
- Accessories REQUIRE a battery harness
- Note: This controller is discontinued and no longer being manufactured
Pre-Nexus controller

- Compatible only with Mobile Link 4G LTE and CDMA Cellular accessories
- Functional only in Mobile Link Consumer App
- NO Command Options
- Exercise Schedule Setting available on LIMITED models
- Note: This controller is discontinued and no longer being manufactured
See also