Salesforce

What type of oil should I use in my home backup generator?

« Go Back
Fields
What type of oil should I use in my home backup generator?
What-Type-of-Oil-Should-I-Use-in-My-Home-Backup-Generator
Content

Read the manual thoroughly and understand all of the instructions, cautions, and warnings before using this equipment. If any section of the manual is not understood, contact your nearest authorized dealer, or contact Generac Customer Service at 1-888-436-3722 (1-888-GENERAC), or www.generac.com with any questions or concerns. 

Selecting generator oil

Generac home standby generators ship from the factory with oil already in the engine. This article provides guidance on what oil should be used after oil changes, and how often it should be changed.

Environment

This article applies to air cooled and liquid cooled home standby generators.

Which oil?

After the 25 hour break-in period (and at every interval there-after), it is recommended to use Generac's proprietary full synthetic 5W-20 Gaseous Engine Oil (GEO) for continuous use. It is specifically formulated for use in gaseous powered Generac generators.

Note: The unit comes filled with 5W-30 weight organic oil (non-synthetic) from the factory. Check oil level and add appropriate viscosity and amount of oil if necessary.


Need the oil capacity for your specific model?
See here: What is the oil capacity of a home standby generator?

 

OilTemperature RangeUse
5W-30Full operating rangeFactory fill and break-in only
Generac Synthetic
5W-20 GEO
Full operating rangeRecommended after break-in
Synthetic 5W-30*Full operating rangeAcceptable (emergency)
10W-30*−10°F to 40°F (−23°C to 4°C)Acceptable (emergency)
SAE 30*> 32°F (0°C)Acceptable (emergency)

* Use only if Generac 5W-20 GEO is unavailable and oil meets API SJ, SL, or better.

Break-in note:
The generator is shipped with conventional 5W-30 oil for the break-in period. Do not switch to synthetic oil until after the initial 25-hour oil change.
Post break-in note:
After break-in, always use Generac’s proprietary full synthetic 5W-20 Gaseous Engine Oil (GEO) whenever possible. If it is unavailable, select an acceptable alternative based on your temperature range and ensure it meets API Service Class SJ, SL, or better.

Oil changes

See also 


Powered by