Follow these button presses to set the controller language:
1. Press ESCAPE until the menu options stop changing (this indicates the user it at the top of the menu tree). 2. Use the arrow keys to navigate to the menu option in the lower right-hand corner, then press ENTER. 3. Use the arrow keys to navigate to the menu option in the lower left-hand corner, then press ENTER. 4. Languages appear in this order:
1. English 2. Swedish 3. Italian 4. German 5. Finnish 6. Dutch 7. Danish 8. Portuguese 9. French 10. Spanish
5. Press ENTER, then use the up and down arrow keys to select a language, then press ENTER.
Power Zone 410
Follow these button presses to set the control panel language:
1. Press OFF and then ESCAPE.
2. Use the DOWN ARROW to navigate to the Settings icon, shown as two gear wheels. Press ENTER. 2. Select Set Language by pressing the DOWN ARROW twice, then press ENTER. 3. Use the DOWN ARROW to select the desired language, then press ENTER. 4. Languages appear in this order:
1. English 2. Spanish 3. Portuguese 4. French 5. Italian 6. Russian 7. Romanian 8. Polish
9. Swedish
10. Finnish
5. After selecting the language, return the generator to AUTO by pressing ESCAPE, then pressing the AUTO button.