Mobile Link device compatibility
Mobile Link can be accessed in two ways: The web app that runs in a browser (app.mobilelinkgen.com ) and the mobile app developed for iOS and Android devices. If you want to run Mobile Link on a laptop or desktop PC, use app.mobilelinkgen.com . If you want to run Mobile Link on your mobile device, us the iOS or Android mobile app.
Mobile Link mobile app phone compatibility
Mobile Link will not run on all smartphones. The Android or iOS device must be running a current or recent version of those operating systems. Mobile Link is guaranteed to be supported and tested for the current version of the OS and 2 previous versions; beyond that, we cannot guarantee compatibility. Current software on devices as of October 2025:
- Mobile Link - 3.11.0
- Android - 16.0
- Apple - 26.0.1
How can I check which OS version my iOS or Android device is running?
See: How to find the software version of an Apple (iOS) or Android device
Mobile Link web app compatibility
Unlike the mobile app, the operating system is not as important for the web app. The web app only runs in a web browser. Currently supported browsers are:
- Google Chrome
- Safari
- Microsoft Edge
Trying to connect to your generator without the Mobile Link app, or on an unsupported device?
- First, try updating the operating system of your device. See this article for operating systems that Mobile Link can run on: What devices can the Mobile Link app run on?
- If your device cannot be updated to the minimum required operating system, consider upgrading the device.
- Try connecting to your generator using the IP method detailed here: Connect a generator to a home Wi-Fi network using a web browser (legacy method)