Salesforce

What does it mean when my generator displays an alarm: Battery Problem, Error Code 2760

« Go Back
Fields
What does it mean when my generator displays an alarm: Battery Problem, Error Code 2760
What-does-it-mean-when-my-generator-displays-an-alarm-Battery-Problem-Error-Code
Content

Read the manual thoroughly and understand all of the instructions, cautions, and warnings before using this equipment. If any section of the manual is not understood, contact your nearest authorized dealer, or contact Generac Customer Service at 1-888-436-3722 (1-888-GENERAC), or www.generac.com with any questions or concerns.

Battery Problem: Error code 2760


Environment

This error applies to error code 2760, BATTERY PROBLEM, for air-cool home standby generators.

Note: The term "error code" is used interchangeably with 'alarm code,' 'fault code,' 'fault alarm' and similar terminology. Error code applies to all such terminology. 

 

Overview

  • Error Codes: 2760
  • Alarm: Battery Problem
  • Issue: At the end of a charge cycle the battery is above 16 volts or is providing more than recommended charge current.
  • Cause: This could be the result of an issue with the battery charging circuit.

 

What can I do?

  • Your options are limited beyond performing basic checks on components and verifying that everything appears normal. You can attempt to clear the alarm and manually restart the unit. 
  • Sometimes, clearing the alarm and attempting to restart the unit is all that is needed, as the alarm may be a one-time occurrence that does not indicate a persistent issue. 
  • How Do I Clear an Error or Alarm Code On My Home Standby Generator?

Note: Generac support does NOT recommend end users attempt to modify or service internal generator wiring. Generac independent authorized service dealers are trained to service Generac generators and can be contacted using the dealer lookup tool on Generac.com: https://www.generac.com/dealer-locator 

 

When should you contact a Generac Independent Authorized Service Dealer (IASD)?

If issues persist after performing the checks and attempting to restart, contacting a Generac IASD for diagnosis is strongly recommended. 

 


Powered by