What is Cold Smart Start?
Cold Smart Start is a feature that helps a home standby generator start more reliably in cold temperatures by monitoring ambient temperature and adjusting its warm-up time. If the ambient temperature is below a fixed temperature upon startup in AUTO mode, the generator will warm up for 30 seconds, allowing the engine to warm before the load is applied. If the ambient temperature is at or above the fixed temperature, the generator will start up with a normal warm-up delay of five seconds. The Cold Smart Start feature is factory-enabled by default, but can be disabled if desired.
Environment
This article applies to Generac air-cooled home standby generators.
For Next Generation Series generators, see here.
For Guardian Series generators (2017-present), see here.
If the ambient temperature is below the 50° F (10° C) upon startup in AUTO mode, the generator will warm up for 30 seconds, allowing the engine to warm before the load is applied.

How do I disable Cold Smart Start?
For Next Generation Series generators, Cold Smart Start can be disabled/enabled in the Field Pro app.
If the ambient temperature is below the fixed temperatures (based on generator size) upon startup in AUTO mode, the generator will warm up for 30 seconds, allowing the engine to warm before the load is applied.

How do I disable Cold Smart Start?
For Guardian Series generators, Cold Smart Start can be disabled/enabled at the generator control panel by following the sequence below. For a visual of the Evolution 2 control panel menu map, see here: Evolution 2.0 controller menu map.
- The screen should display READY TO RUN. Press the ESC button.
- Using the up/down arrows, Toggle the controller to SUB MENUS and press the ENTER button.
- Toggle to the EDIT option. Press ENTER.
- Language should be displayed. Toggle to the Cold Smart Start? option.
- To disable, toggle to NO and press ENTER. To enable, toggle to YES and press ENTER.
Note: if the control panel display is not blinking or flashing to indicate your selection, see here: Why is my control panel display not flashing or blinking to indicate the selected menu?