Schedule A maintenance
Home standby generators require specific maintenance tasks to be completed at different intervals to prolong the life of the generator and keeping it in good working order. Schedule A maintenance refers to a collection of tasks that should be performed every two years or every 200 hours of operation, whichever comes first.
When the Schedule A maintenance interval has been reached, the status light on the side of the generator will turn yellow: What Does a Shining Yellow LED Light Mean on the Control Panel of My Generator?
Environment
This article applies to:
- Generac Next Generation Series 10-28 kW air-cooled standby generators
- Generac Guardian Series 10-26 kW air-cooled standby generators (2017 to present)
When the Schedule A Maintenance interval has been reached:
- Guardian series generators will display a yellow LED status light, and the control panel will state SERVICE A.
- Next Generation series generators will display a yellow LED status light, and a notification stating SERVICE A will appear in Mobile Link.
Schedule A maintenance tasks
Note: Generators that operate in extremely hot or cold environments <40°F (<4.4°C) or >85°F (>29.4°C) will require an oil and oil filter change after every 100 hours of run time since last service, due to the strain that extreme environments put on the engine and fuel system.
Who can perform maintenance?
Homeowners can perform regular maintenance tasks as outlined in their generator's user manual. Alternatively, homeowners can contact a Generac authorized service dealer for help. See Where Can I Find a Company to Perform Standard Maintenance On My Generator? for more information.
Regardless of who performs the maintenance, maintenance records must be kept for future reference. The Mobile Link for Generators app offers functionality to record and track maintenance tasks. See the Viewing, Adding, Deleting, & Exporting Maintenance Schedule Records in Mobile Link article for more information.
After maintenance procedures have been completed, follow the post-maintenance check procedure to ensure the home standby unit is "ready to run": How do I perform post maintenance checks on a home standby generator?
Lastly, clear the Schedule A Maintenance warning the same way you clear an error code:
1. Press the red OFF button
2. Press ENTER 2 times for each maintenance alarm present. There may be more than one maintenance alarm; press ENTER to acknowledge and clear each alarm for which maintenance has been completed.
3. Press the green AUTO button. This will return the unit to automatic standby mode.
1. After maintenance procedures have been completed, follow the post-maintenance check procedure to ensure the home standby unit is "ready to run": How do I perform post maintenance checks on a home standby generator?
2. Then, clear the Schedule A Maintenance warning by selecting "Clear Maintenance" in the Mobile Link app. Alternatively, you can clear the warning at the generator control panel by pressing and holding the OFF button for 3 seconds.
3. Lasty, document the maintenance performed: Viewing, Adding, Deleting, & Exporting Maintenance Schedule Records in Mobile Link
See also